A Few questions in L9780 "Wide range air fuel sensor control interface"
- September 17, 2018
- 7 replies
- 5810 views
We are developing a system which uses a
Wide range air fuel sensor control IC "L9780" which is planned to be interfaced to the Bosch LSU4.9 Probe Sensor. We have worked previously with Bosch's CJ125 and planning on going over to use ST's L9780, but we need to fill in the gaps to proceed.
In the datasheet ( the only document available ) The application notes is missing a lot of basic information.
I've contacted ST Microelectronics, but seems they have nothing to help filling the gaps.
I would appreciate if someone would kindly help us out. I'm willing to share more information if desired. My questions so far are as follows :
1- No details on how to calculate the Nernst cell impedance from the RCT2 amplifier readings
2- No information about the how the impedance measurement is used in the heater PID control program
More to come later if we can find an expert to answer or application notes.
Regards
Sultan