Skip to main content
PJ.3
Visitor II
April 8, 2022
Question

AUDIO_OUTPUT_BUFF_SIZE Bit mismatch while separating audio data from 4 channels TDM data. (Audio data extraction and processing on AMicArray_Microphones_Streaming demo example)

  • April 8, 2022
  • 0 replies
  • 484 views

I have been studying the x-cube-memsmic1's AMicArray_Microphones_Streaming example. I have used 4 channel mic array expansion module.

As per the theory, incoming data is from 4 channels, 16-bit slot size per channel, and 96khz sampling frequency. so the incoming data per millisecond should be of size 96000/1000 * 4 = 384 (uint16_t).

However, in the demo example, the AUDIO_OUTPUT_BUFF_SIZE  has doubled the intended buffer size.

#define AUDIO_OUTPUT_BUFF_SIZE ((AUDIO_IN_SAMPLING_FREQUENCY/1000)*AUDIO_IN_CHANNELS*2)

My question is how the AUDIO_OUTPUT_BUFF_SIZE is calculated here?

Another question is incoming data are slot1, slot2, slot3 and slot4. and the data is in MSB first configuration with a 16-bit slot size. So can we extract per channel data in a separate buffer?

How can we further process it as it is in PCM format? Is there any documentation available for general steps to follow?

    This topic has been closed for replies.