Skip to main content
Snara.21
Senior
October 20, 2021
Question

I am using Steval-mksbox1v1. I need a sample code or standard library , application notes and programming manual for Microphone TS922EIJT and MP23ABS1TR

  • October 20, 2021
  • 0 replies
  • 493 views
  1. How to configure ADC in STEVAL - MKSBOX1v1 (With DMA or W/o DMA)
    1. How are the setting to be used for this board. (Clock dividing by ?) - For Audio it will be single channel continuous scan
    2. There are two pins in STEVAL - MKSBOX1V1 MREF and M1P what should I do that in MX and in the firmware function
    3. Whether any firmware logic is there for ADC Microphone if so please share the reference. If I create the [roject it has to work with the code I create, so please share the [rogramming manual for Analog Microphone
  • Like
  • Reply
  • Select as Best

    This topic has been closed for replies.