LM2901 with one input outside the input common mode range
In the data sheet for TSX339 it says in chapter 6.1:
"The output state is guaranteed as long as one input remains within the common mode
input voltage range (defined in the operating conditions table), and the other input remains
between -0.3 V and 16 V (meaning that one input can be driven above VCC+)."
Is the same true for LM2901, i.e. one input within the common mode input voltage range and the other input between -0.3 V and 36 V?