Poblem with LM358DT and not with LM324AD
Dear all, the first of all thanks for let me leave a message in this post.
We have a schematic circuit, with the LM324 it works but with the LM358 doesn´t work. It gives the correct voltage in both chips in the output, I connect a relay solid state from Carlos Gavazi and with the LM324 works and with the LM358 doesn`t works. the differents inside the chips are ( picture attach).
I check the mA output and all is correct. the consume of solid state relay is only 10mA
Somebody have this error?
Which difference the are between the LM324 and LM358? could somebody give me a refference form a LM324 in two cannels? thanks in advanced

Thanks in advanced.