TSC888A gain is low
I'm using the TSC888A current sensing amplifier in BLDC (brushless DC) motor controller current limit circuit. I'm seeing a gain of about 10 from the amplifier instead of the published typical value of 20. The data sheet does not specify a min or max gain but does state an output accuracy of 6%. With a 0.05 ohm series resistor and 1.2A current I am seeing an output voltage of 650mV. According to my calculations I should be seeing 1.2V (1.2*0.05*20).
Vcc and Vp are both connected to same 12V power bus.Has anyone else seen this problem? #tsc888