Question
TSV632 - negative input current allowed?
Posted on June 27, 2013 at 11:53
Hello,
the datasheet for the OpAmp TSV632 allows a maximum input current of 10mA (page 4).There's no sign given, so I suppose negative input currents aren't allowed.. But I'm not sure and it would help me, if they would be allowed..So, could someone clarify this, please?I have series resistors in front of the inputs which would limit the input current to -0.6mA in the worst case.. But I also noticed the input voltage dropping under the allowed Vcc- -0,2V, so it looks for me as current limiting is not enough and I also have to limit the voltage..Thanks in advance,Christian #amplifier-input-protection