Skip to main content
DHwan.5
Associate
August 17, 2021
Question

What is the range of frequency that 1N5711 schottky diode can operate? (Right Switching Action) (ex. 100MHz ~ 10GHz) OR What is the range of Reverse Recovery Time of 1N5711 diode?

  • August 17, 2021
  • 1 reply
  • 1452 views

..

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    Technical Moderator
    August 18, 2021

    Welcome, @DHwan.5​, to the community!

    the reverse recovery time of Schottky diodes is determined by two factors: the inductance of the external wiring and the internal junction capacitance, which is why it cannot be included in the datasheet. Beside the given junction capacitance, the maximum switching speed therefore depends heavily on your layout.

    If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

    /Peter

    DHwan.5
    DHwan.5Author
    Associate
    August 20, 2021

    Please see my new question!! I offered my additional information.