Cannot run program ''make''
Hello,
I installed SPC5 Studio and everything works fine and then after a view hours of working, i can´t build my project any more. I am always getting following error and i don´t know why:make -j4 all
Cannot run program ''make'': Launching failed12:30:14 Build Finished (took 47ms)
I did not change anything in the settings, just using the SPC5 Studio as it is configured after the installation. But this error seems to come up randomly after a while. So i re-installed SPC-Studio several times. After the installation it worked again and I was able to build my projects. But during working on my code a get the same error again and again after a while.
What could be the reason for that error upcoming randomly? I am using the 30days evaluation license from High-Tec.