Skip to main content
prashanth.mohan22
Associate III
May 23, 2019
Solved

Confused between set address for bootloader and 32-bit store address from UART/CAN flash while flashing

  • May 23, 2019
  • 1 reply
  • 744 views

Hi,

This is for SPC560Bxx. I need clarification on set address for bootloader and the 32-bit address that shall be mentioned on UART/CAN frame.

There is one column in firmware updater component, where we are supported to choose it the set address, here 0x0010000 or 0x0018000, yes, it is mentioned in 28-bits. There shall be another address sent via UART/CAN line, in step 2 of boot process after valid password verification.

I got bit confused here and would like to have a clarification on both its usage.

So,

  1. What is the set address, we are speaking about in firmware updater component?
  2. What is the range of load address that can be used for SPC560B54L5? And this is a 32-bit address.

Thanks for your time on helping me out.

Regards,

Prashanth

    This topic has been closed for replies.
    Best answer by Erwan YVIN

    Hello ,

    have you opened the Document (PDF-PowerPoint) in the document ?

    It is very useful to understand the component.

    0690X000009YqUtQAK.png

    More information are in the RM

    Best regards

    Erwan

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Employee
    July 17, 2019

    Hello ,

    have you opened the Document (PDF-PowerPoint) in the document ?

    It is very useful to understand the component.

    0690X000009YqUtQAK.png

    More information are in the RM

    Best regards

    Erwan