Skip to main content
NBula.1
Associate III
September 25, 2020
Solved

Debugging with SPC5Studio and UDE

  • September 25, 2020
  • 3 replies
  • 4022 views

Hi,

I am trying to upload a code to my SPC570S-DISP development board, but I am having an issue with the debugging tool UDE. I searched for this issue in the forum and I have tried all the solutions given and none of it work. When I try to debug from SPC5Studio I get this error,

0693W000004HAWCQA4.png

And when I try to use the UDE STK tool I get this error,

Message from component 'PpcJtagTargIntf' :

Can't connect target !

Message from component 'PpcJtagTargIntf' :

No JTAG client found !

Please check:

- target power supply

- JTAG cable connection

- target configuration

I have created a case with ST, and so far no one has been able to figure out what the problem is. As I saw from the posts in the forum, many users are having this problem. Please be kind enough to look into this matter.

    This topic has been closed for replies.
    Best answer by Erwan YVIN

    Hello ,

    Average Power Output :

    The average power of a USB port is about 5 volts. Your USB device will be able to draw out a maximum of 500 milliamperes (mA), but most default to 100 mA until prompted to provide more power by the device software. FTDI Chip and the board require more power than 500 mA, it may work not at all while plugged into your computer.

    could you plug the USB Cable into USB Port of your Laptop (High Power) ?

    Best regards

    Erwan

    3 replies

    Erwan YVIN
    ST Employee
    September 30, 2020

    Hello ,

    PLS Eclipse Plugins (32 bits) and SPC5Studio 6.0 (64bits) last eclipse ecore are not compliant anymore.

    it worked only on SPC5Studio 5.8.1 (32 bits)

    PLS should deliver a new plugin in Q1 202.

    I recommend to use PLS in external use.

    http://www.pls-mc.com/spc5-udestk-udestk

    Please uncheck this option0693W000004ICIOQA4.png

    Best regards

    Erwan

    NBula.1
    NBula.1Author
    Associate III
    September 30, 2020

    Hi,

    I unchecked this option. When the debug button is pressed, the UDE STK software launches. However, no file is opened, only the blank software window. Then I tried opening the debug.wsx and I get this error,

    0693W000004IEIqQAO.png

    I am powering the board using a 12V power supply. Are there any settings that I should change in the target interface setup? I have uploaded the connection error log. I tried changing the .cfg file in the debug.wsx file from "spc570s_discovery_debug_jtag.cfg" to "stm_spc570s50_velvety_discovery_starterkit_debug_jtag.cfg" since it was stated in one of the discussions. I followed the steps to setup the VCP port for the device as well.

    0693W000004IELKQA4.png

    I contacted PLS as well. And according to them, it is a power issue. Please help me in this matter.

    Thank you.

    NBula.1
    NBula.1Author
    Associate III
    October 5, 2020

    Hi,

    A reminder about the question I asked

    Erwan YVIN
    ST Employee
    October 7, 2020

    Hello ,

    I am checking with the board in the lab bench. (spc570s_discovery)

    Could you send me the version of your board ?

    Best regards

    Erwan

    NBula.1
    NBula.1Author
    Associate III
    October 7, 2020

    Hi Erwan,

    Thank you for the reply. In the product delivery note it says the Release version is 1.0.

    Don' t know whether this is the correct value.

    Nisal

    Erwan YVIN
    ST Employee
    October 13, 2020

    Hello ,

    i had a similar problem.

    In plugging the USB cable to USB port (High Voltage).

    i can flash and debug.

    could you plug the USB Cable into USB Port (High Voltage) ?

    Best Regards

    Erwan

    NBula.1
    NBula.1Author
    Associate III
    October 13, 2020

    Hi Erwan,

    I am not clear. Could you explain what I should do?

    Nisal

    Erwan YVIN
    Erwan YVINBest answer
    ST Employee
    October 13, 2020

    Hello ,

    Average Power Output :

    The average power of a USB port is about 5 volts. Your USB device will be able to draw out a maximum of 500 milliamperes (mA), but most default to 100 mA until prompted to provide more power by the device software. FTDI Chip and the board require more power than 500 mA, it may work not at all while plugged into your computer.

    could you plug the USB Cable into USB Port of your Laptop (High Power) ?

    Best regards

    Erwan