Do I need to complete the components on the SPC58EC-DISP development board?
In the schematic of the ethernet configuration it is indicated that 3 components are not assembled: R28, R33 and R120. My question is, should I solder them for it to work?
In the schematic of the ethernet configuration it is indicated that 3 components are not assembled: R28, R33 and R120. My question is, should I solder them for it to work?
Hello,
from README.TXT
It needs to configure the network component providing the networking configuration:
i.e: MAC Address, IP static Address.
Open a console and ping from a remote host to the IP address configured for the board.
Fit the following jumpers to configure the network:
JP5:
ETH_PWR -> [3 - 4]
RESET -> [5 - 6]
ETH_TX_CLK -> [7 - 8]
ETH_TXD_0 -> [9 - 10]
ETH_TXD_1 -> [11 - 12]
ETH_TXD_2 -> [13 - 14]
ETH_TXD_3 -> [15 - 16]
ETH_TX_EN -> [17 - 18]
ETH_MDIO -> [19 - 20]
ETH_MDC -> [21 - 22]
ETH_COL -> [23 - 24]
ETH_CRS -> [25 - 26]
ETH_RX_ER -> [27 - 28]
ETH_RX_DV -> [29 - 30]
ETH_RXD_0 -> [31 - 32]
ETH_RXD_1 -> [33 - 34]
ETH_RXD_2 -> [35 - 36]
ETH_RXD_3 -> [37 - 38]
ETH_RX_CLK -> [39 - 40]
JP50: FIT
Do not forget to plug a cable.
Regards.
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.