Skip to main content
Erwan YVIN
ST Employee
December 9, 2019
Question

download.spc5studio.com

  • December 9, 2019
  • 0 replies
  • 712 views

Dear All ,

SPC5Studio updated components are available (56,57 on 58)

more information on http://download.spc5studio.com/

SPC58xHxx, Advanced GTM and USBTypeC credentials should be requested on credentials@spc5studio.com

New or updated components

RLA 1.11.0

   SPC58xHxx : Full support of cut2 Mcan driver without CCCU

   SPC584Bxx: PWM ICU test application

   SPC560Pxx STEVAL-TTM002V1 board support

RLA 1.11.0 and Benchmark 1.4.0

  support of SPC58xH-DISP board with benchmark application

RuntimeIO_1.3.4

   Add mode (ASYNC, SYNC, Buffered) for serial configuration

Firmware updater 1.4.1

   Inversion of CAN buffer

Flash 1.10.1

   Copyrights update

 Best Regards

 Erwan

    This topic has been closed for replies.