Skip to main content
Bwang.3
Associate III
May 15, 2024
Solved

DSPI parameter configuration issue of SPC5

  • May 15, 2024
  • 1 reply
  • 1005 views

Hello! I would like to ask what each of the three modes in the picture below represents?
Also, what does it mean if the GPIO parameter is set to PORT_1? I did not see that the GPIO bit 0 for this PORT_1 port is in use in the pin configuration editor! So I would like to ask if this parameter has been configured and used on this image?
Also, what does this PCS Line mean by choosing PCS1?
Is there a user manual for the parameter settings of DSPI for SPC582B! Because I want to know what the configuration parameters in the routine mean!
QQ图片20240515103352.png
Best answer by Max VIZZINI

Duplicated request in AutoDevKit Forum.

1 reply

Max VIZZINI
Max VIZZINIBest answer
Technical Moderator
May 29, 2024

Duplicated request in AutoDevKit Forum.