eTimer Clock selection
- March 22, 2018
- 1 reply
- 1681 views
Hello Dear Forum members,
This question is regarding SPC560P40L1 controller's eTimer module.
At the moment my eTimer module using 'IP Bus clock' which is of 64M Hz. I am using prescaler value of '32' to get 2M Hz to eTimer module.
I want to have clock frequency of 20M Hz(or 40M Hz or multiples of 20M Hz basically).
I see in the block diagram of technical datasheet that(Please see attachments) there is option to choose from clock sources: 'Clock' or 'IP Bus clock'
The crystal oscillator frequency is 40M Hz. I would like to use this frequency as input to my eTimer module but i don't know how or even it's possible to get this Frequency routed to eTimer ?
I would be happy if someone can share any useful tips or suggestion in this regard.
Best regards
Sathish
#spc5 #spc5x #clock-selection #etimer