Skip to main content
stefanodimascio9
Associate III
November 14, 2015
Question

FCCU configuration

  • November 14, 2015
  • 25 replies
  • 5347 views
Posted on November 14, 2015 at 15:56

Hello everybody, 

I'm using the SPC56EL70L5.Trying to configure the FCCU, I coded:

&sharpdefine CTRLK_OP1 0x913756AF   

&sharpdefine CTRLK_OP2 0x825A132B     //keys needed for operation

&sharpdefine CTRL_OPR1 1    

&sharpdefine CTRL_OPS3 3   

uint32_t FCCU_CONFIG_STATE(void){

    /* ----------------- CONFIG State --------------------- */

    FCCU.CTRLK.R = CTRLK_OP1; /* Key for the operation OP1 */

    FCCU.CTRL.R = CTRL_OPR1;  /* Set the FCCU into the CONFIG state [OP1] */

    while(FCCU.CTRL.B.OPS != CTRL_OPS3);   /* wait for the completion of the operation */

    return 1;

}

But condition is never verified: FCCU.CTRL.OPS is 0x02 (that means operation is aborted) and MCU hangs in the while.

Where is the mistake?

Thanks in advance for the help.

#leopard #fccu #spc56
    This topic has been closed for replies.

    25 replies

    stefanodimascio9
    Associate III
    November 25, 2015
    Posted on November 25, 2015 at 15:18

    Thanks a lot, now it works.

    Best regards

    simone
    Associate II
    February 2, 2016
    Posted on February 02, 2016 at 14:04

    I'm trying to do the same, together with the sample of gpios and UART (see attached file). I get

    0x027F0 -> ''clock failure''

    , even if I added the pre and post lines.

    Thank you.

    ________________

    Attachments :

    main.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Xb&d=%2Fa%2F0X0000000baC%2FyodoxKwCdpe1olPLqBLXb_THDIul1sUQFhU3oIe9Od4&asPdf=false
    simone
    Associate II
    February 2, 2016
    Posted on February 02, 2016 at 15:34

    I think the problem in my case is the use of componentsInit()

    Erwan YVIN
    ST Employee
    February 2, 2016
    Posted on February 02, 2016 at 16:43

    Hello Simon ,

    Did you try the patch that i have provided (above) ?

    (configuration.xml)

         Best regards

                    Erwan

    simone
    Associate II
    February 2, 2016
    Posted on February 02, 2016 at 18:11

    Yes, but it doesn't work if I add the components initialization function. Without is fine.

    simone
    Associate II
    February 3, 2016
    Posted on February 03, 2016 at 16:01

    I attached the call stack. Thank you.

    ________________

    Attachments :

    failurestack.bmp : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0XW&d=%2Fa%2F0X0000000ba9%2FS8bE3yowKV75VTb17byj4YtdpnsX12p77atM2MDCdlA&asPdf=false
    stefanodimascio9
    Associate III
    February 4, 2016
    Posted on February 04, 2016 at 11:03

    Simon,

    I tried to fix the problem, as I'm working on this architecture too. Apparently clock can be reinizializated only in DRUN mode.

    So you have to put componentsInit() after the cleaning of FCCU and the transition from safe to DRUN. I attached some code that successfully inject the fault but it hangs during the transition from SAFE to DRUN and it is reset from software watchdog. I don't know what's the problem there, maybe Wan35fr could be more useful.

    ________________

    Attachments :

    fccu.h : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0WU&d=%2Fa%2F0X0000000baA%2Fcrbqh9IDE6mclmUYbC_hjljaLX3ji__C1ZH1ujDeZC8&asPdf=false

    main.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzg5&d=%2Fa%2F0X0000000ba8%2FBv0MxD5bNEFGa0ljoFr5ibJsLZtPXRUBC.XhVFLZbZY&asPdf=false
    stefanodimascio9
    Associate III
    February 8, 2016
    Posted on February 08, 2016 at 14:21

    The other thing that troubles me in this case is the use of sdStart(): on the first run it works but after the reset it causes the microcontroller to have an unhandled exception, even if needed because the serial is in STOP state. I can't understand the reason.

    Erwan YVIN
    ST Employee
    February 9, 2016
    Posted on February 09, 2016 at 11:07

    Hello Stefano ,

    you can find the MSC linked to the Serial port.

    http://chibios.sourceforge.net/docs3/hal/group___s_e_r_i_a_l.html

    Could you check if your PCTL (LINFLEX0)  is still set ?

    maybe , you are accessing to the address.

    you have to reenable associated PCTL.

           Best regards

                        Erwan

    stefanodimascio9
    Associate III
    February 9, 2016
    Posted on February 09, 2016 at 11:45

    Before the exception, in sdStart(), ME_PCTL48 (LINFLEX0) is anyway set to 0x11. 

    But 

    linflexp->LINCR1.R  = 1;                      /* INIT bit.                */

    0x00001FCE:   48 10        SE_LI     R0,0x1

    0x00001FD0:   B1 0F        SE_STH    R0,0x2(R31)

    still causes the exception after the reset.