Skip to main content
Rajesh kumar
Visitor II
March 9, 2017
Solved

Hi i am working on Project with a SPC560D40 an SPC5 Studio. I'm trying to generate PWM-Signals on the Pins RA0 to RA5. When I look in the eMIOs Settings of the SPC560Dxx HAL Driver Component, I can only activate eMIOs group 0 (Channel 9..15) or Group

  • March 9, 2017
  • 1 reply
  • 877 views
Posted on March 09, 2017 at 08:14

hello i am working on Project with a SPC560D40 an SPC5 Studio. I'm trying to generate PWM-Signals on the Pins RA0 to RA5. When I look in the eMIOs Settings of the SPC560Dxx HAL Driver Component, I can only activate eMIOs group 0 (Channel 9..15) or Group1 (Channels 17..23) but RA0 to RA5 should be Channel 0..5. For these Channels I can only activate ICU drivers.

    This topic has been closed for replies.
    Best answer by Erwan YVIN
    Posted on March 09, 2017 at 10:44

    Hello Rajesh ,

    yes , it is our HAL Drivers implementation.

    you can use patch mode to update our HAL drivers

    icu_lld.c or pwm_lld.c directly in SPC5Studio.

    or contribute in 

    https://github.com/microwan/spc5-hal

     

                                 Best Regards

                                                Erwan

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Employee
    March 9, 2017
    Posted on March 09, 2017 at 10:44

    Hello Rajesh ,

    yes , it is our HAL Drivers implementation.

    you can use patch mode to update our HAL drivers

    icu_lld.c or pwm_lld.c directly in SPC5Studio.

    or contribute in 

    https://github.com/microwan/spc5-hal

     

                                 Best Regards

                                                Erwan