Question
Hi, I've created a time for one second and transmitting CAN over the one side task. But the CAN message is not transmitted one second once, instead it is transmitting continously with IFS. What might be wrong in my code? please clarify
uint8_t pit_ch1_var=0;
uint32_t pit_ch2_var=0;
void pit_ch1_cb(void)
{
pit_ch1_var = 1;
}
void pit_ch2_cb(void)
{
pit_ch2_var++;
}
/*
* Application entry point.
*/
int main(void) {
CANTxFrame txmsg;
CANTxFrame txmsg1;
/* Initialization of all the imported components in the order specified in
the application wizard. The function is generated automatically.*/
componentsInit();
/* Enable Interrupts */
irqIsrEnable();
/* Start PIT driver */
pit_lld_start(&PITD, pit_config);
/* Enable PIT Channels */
pit_lld_channel_start(&PITD, 1U);
/*
* Activates the CAN driver 1.
*/
can_lld_start(&CAND1, &can_config_cfg0);
/*
* CAN TX Message structure.
*/
txmsg.IDE = CAN_IDE_STD;
txmsg.RTR = CAN_RTR_DATA;
txmsg.LENGTH = 8U;
txmsg.data32[0] = 0x55AA55AAU;
txmsg.data32[1] = 0x00000000UL;
txmsg1.IDE = CAN_IDE_STD;
txmsg1.RTR = CAN_RTR_DATA;
txmsg1.LENGTH = 8U;
txmsg1.data32[0] = 0x00000000UL;
txmsg1.data32[1] = 0x00000000UL;
/* Application main loop.*/
while(1)
{
if(pit_ch1_var == 1)
{
pit_ch1_var = 0;
txmsg.IDE = CAN_IDE_STD;
txmsg.SID = 0x100;
while (can_lld_transmit(&CAND1, 1, &txmsg) == CAN_MSG_WAIT) {
}
txmsg1.SID = 0x100;
while (can_lld_transmit(&CAND1, 1, &txmsg1) == CAN_MSG_WAIT) {
}
pal_togglepad(PORT_C,PC_LED8);
}
else
{
pal_togglepad(PORT_C,PC_LED7);
}
}
return 0;
}How to transmit can as per the cycle time requirements, 10ms, 100ms or 500 ms. Please clarify.