Hightec compiler problem with SPC5Studio
Hello everyone,
I have a problem with the Hightech compiler used in SPC5Studio, I try to explain my issue: on my PC I have installed the SPC5Studio v5.0.0 and the Hightec compiler toolchain v4.6.6.1.
I configured the SPC5 Studio to use the Hightech compiler by adding the following values in the PATH:
C:\HighTec\toolchains\powerpc\v4.6.6.1\bin;
C:\HighTec/licensem
situated under
Windows -> Preferences ->C/C++ -> Build -> Environment (see the attachment )

I made a test project, builded it and all worked fine, but if I close the SPC5 Studio then reopen it and build again the project (after a clean) the buildin doesn't work anymore; I checked under
Windows -> Preferences ->C/C++ -> Build -> Environment and the values:
C:\HighTec\toolchains\powerpc\v4.6.6.1\bin;
C:\HighTec/licensemanager
were missing in the PATH, the only way to make it work is to copy again in the PATH these two values.
Then I tried to add a new variable and copy in it the two values, but it didn't work too.
I'm asking if there is a way to avoid the copy of the values every time I close and open the SPC5 Studio.
Thank you in advance.
Stefano Maccari