Skip to main content
michel_hoehn
Associate II
September 11, 2019
Question

How to adjust Flex Pwm registers for a variable pwm-frequence?

  • September 11, 2019
  • 0 replies
  • 615 views

Hi,

I´m trying to implement the synchronous pulse width modulation for my Bachelor-Thesis. Therefore the frequency of the pulse width modulation is variable.

I´m using the  SPC560P44Lx, SPC560P50Lx microcontroller family.

So what I want to do is to adjust the Registers where the frequency is stored as the peak value of a counter.

This is how my 3 Flex Pwm submodule-registers are initialized;

for.....{

 FLEXPWM_0.SUB[u08_counter].CTRL.R     = 0x0400U;

 FLEXPWM_0.SUB[u08_counter].CTRL2.R    = 0x2000U;

 FLEXPWM_0.SUB[u08_counter].DTCNT0.R   = 50U;   

 FLEXPWM_0.SUB[u08_counter].DTCNT1.R   = 50U;   

 FLEXPWM_0.SUB[u08_counter].INIT.R     = 0xF7A1; <------ This Value has to be adjusted every sampling period

 FLEXPWM_0.SUB[u08_counter].VAL[0].R   = 0x0019U;

 FLEXPWM_0.SUB[u08_counter].VAL[1].R   = 0x085FU; <------ This Value has to be adjusted every sampling period

 FLEXPWM_0.SUB[u08_counter].VAL[2].R   = 0x0U;  

 FLEXPWM_0.SUB[u08_counter].VAL[3].R   = 0x0U;  

 FLEXPWM_0.SUB[u08_counter].DISMAP.R   = 0x00FFU;

 FLEXPWM_0.SUB[u08_counter].OCTRL.R    = 0x0000U;

}

  // Load the PRSC bits of CTRL1 and the INIT, and VALx registers into a set of buffers

  FLEXPWM_0.MCTRL.B.LDOK = FLEXPWM_0_MCTRL_LDOK_LOAD_ALL;

  // Fault registers setting

  // Set the filter register to inactive

  FLEXPWM_0.FFILT.R = FLEXPWM_0_FFILT;

  // Clear the Fault flags

  FLEXPWM_0.FSTS.R = FLEXPWM_0_FSTS_RESET;

  // Set the Fault Control Register

  FLEXPWM_0.FCTRL.R = PWM_FLT_CTRL_OFF;

Do I have to do the whole initializing process or is it possible to just adjust the the marked registers? If I can adjust these 2 registers, how? I´m new to this Chip and Software and I really reached the point of not knowing what to do.

Thank you for your help.

Best regards,

Michel

    This topic has been closed for replies.