How to use SPC5-FLASHER
Hi,
I am trying to use SPC5-FLASHER, in particular the version SPC5FlashProgrammer2.7.9, in order to manage the Flash using the BAM/BAF functionality, but I am having troubles. Firstly, the target board I am employing has the microcontroller SPC570S40E1. This one isn't present among the options in the "Configuration" tab, so I was wondering if the device SPC570S50, which belongs to the same family of mcus, is a good choice or not.
Futhermore, I programmed the target board with the project “SPC570Sxx_RLA Bootloader Application for Discovery�?, which I obtained in the following way:
- I created a new project File/New/ SPC5Studio import wizard/
- I selectedthe family SPC57
- I selected the evaluation board SPC570S50L1DISP
- I selected the Application “SPC570Sxx_RLA Bootloader Application for Discovery�?
At startup the boatloder should wait for host connection ( I selected via UART) for firmware downloading. . Is it ok to use this project in order to use SPC5-FLASHER?
Doing in this way, selecting this configuration:

and selecting as interface UCUART:HybridCom/4/UART, when I try to connect, I get:

How can I fix this problem?
Francesco.