How to wakeup the system after few Hr's when system is in Stanbymode.
Hello Team,
This is Shivananda from Robert BOSCH. we are using SPC584Cx/SPC58ECx 32-bit MCU family (Chorus 4M).
we need to implement a feature when system in stanbymode, after 5 hours self wakeup of system should happen.
Hope using Timer/Counter concept we need to achieve 5 hours count and also using '
Smart Standby Wakeup unit� (SSWU) we can Wakeup the system.
As per reference manual I have this information
IRCOSC is also the system clock available during the STANDBY and it is placed in
STANDBY power domain.
Is it possible to implement this feature in Chorus4M???? if Pls can anyone help me in this to implement this feature.
- I need Register details which are required to achieve this
1. How to run timer in stanbymode and which and how to enable clock to run the timer.
2. After 5 hrs. of time how can I wakeup the system( which registers need to program).
Thanks and Regards,
Shiva
9739636666
#standbymode #automotive #sleep-wakeup #lowpower-sleep