I would like to know how to add the CAN receive function for CAN_6 in SPC582B Discovery Board.
In the SPC582B Discovery Board (QFP64 package), I need to use CAN_6_RX and CAN_6_TX which are in the uC pin 63 and 64. But when I used the CAN Test Application, I cannot find the CAN Driver related to the CAN_6. How would I program the CAN_6 protocol receive function? I have already done the complete and error-free code for CAN_2 and CAN_1. Hope to hear from you soon.