Skip to main content
Visitor II
March 27, 2025
Question

Issue: DSPI_0 Mapping Fails with "Bad Clock Setting" Error

  • March 27, 2025
  • 0 replies
  • 401 views

I am configuring the SPI module in EB Tresos and attempting to map DSPI_0 in the unit hardware mapping section. However, I receive a bad clock setting error for DSPI_0.

The same error occurs for all DSPI units except DSPI_4 and DSPI_5, which do not show any issues. My port pins and clock configurations are set for DSPI_0, so I expect it to work correctly, but it fails.

Environment:

  • Microcontroller: SPC58NN84E7

  • Tool: EB Tresos

  • Module: SPI Driver

  • Error Message: "Invalid value for node 'SpiPhyUnitMapping': DSPI Hw unit has bad DSPI_CLK settings."

Has anyone encountered this issue before? Could there be a missing configuration step for DSPI_0’s clock settings in EB Tresos? Any suggestions on what else to check?

Thanks in advance!