Skip to main content
VPAI.1
Associate
July 16, 2020
Solved

Issue in Flashing the SPC584B- DSM board

  • July 16, 2020
  • 2 replies
  • 1283 views

Hi Team,

Please help to resolve the issue

Flashing the SPC584B- DISP board failed and end up in the following errors,  

Error messages:

 PpcJtagTargIntf: Connection to target lost !

 PpcJtagTargIntf: Failed to reset target system !

 PpcJtagTargIntf: No JTAG client found !

Please check:

- target power supply

- JTAG cable connection

- target configuration 

  • This issue has started just after connecting with external LIN device(NeoVI Blue).
  • All indicator LEDs in the board are still glowing.
  • The device is still visible in Device Manager under Ports on connecting with the computer.
  • There is no fluctuation in the current observed.
  • The power is given through regulated power supply keeping maximum current 200mA.

Regards

Sudeendra S

    This topic has been closed for replies.
    Best answer by Erwan YVIN

    Hello Sudeendra ,

    Could you install the PLS drivers located in UDE Folder

    c:\Program Files (x86)\pls\UDE Starterkit 4.10\Driver\JtagUsbDriver\ ?

    Best Regards

    Erwan

    2 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Employee
    July 17, 2020

    Hello Sudeendra ,

    Could you install the PLS drivers located in UDE Folder

    c:\Program Files (x86)\pls\UDE Starterkit 4.10\Driver\JtagUsbDriver\ ?

    Best Regards

    Erwan

    VPAI.1
    VPAI.1Author
    Associate
    July 17, 2020

    ​Hi Erwan,.

    Thanks allot.Resolved the issue by the suggestion provided.

    Regards

    Sudeendra s