Skip to main content
Associate III
July 30, 2023
Question

L9963 Evaluation Board with GUI does not work

  • July 30, 2023
  • 2 replies
  • 3113 views

Hello!

I performed the steps in manual to get it started. I could assign an ID and I could get the green ACK. 

As soon as I try to go to the next step (3.2) configuring voltages the ACK turns red. Meaning I can´t send any configs to the device. I tried to read instead of writing, same outcome. 

Sometimes I can get the ACK green again if I start diagnostic, sometimes I need to powercycle. 

I connected the minimum pack voltage ( 2 cables) and I also tried the 4 cell connection with resistors- same outcome. 

Open wire detection tells me only the first and the last cell are connected (after that the ACK for that button also turns red) 

The attached AN states it should be Firmware 1.6...is there a new firmware? I have 1.5 (as the picture in the AN also shows) I can+t find any manual showing how to update the firmware. 

What am I missing? 

This topic has been closed for replies.

2 replies

RhSilicon
Lead
July 31, 2023

I was surprised that the page about this device seems to be incomplete, (I expected at least the full IC datasheet) and unfortunately I found this, in the software section: "Not recommended for new designs".

L9963.png

https://www.st.com/en/automotive-analog-and-power/l9963.html#tools-software

OrbiterAuthor
Associate III
July 31, 2023

What?! This was not there a few days ago... but its only the Eval board, not the chip, the chip is still green and it should be for 10 years now. L9963E - Automotive chip for battery management applications with daisy chain up to 31 devices - STMicroelectronics

But still, I purchased it, I payed, i would like to use it... 

OrbiterAuthor
Associate III
July 31, 2023

Does someone have a download link to the GUI software? 

I may have loaded the one for L9963E by accident. 

And I cant find the one for L9963

 

July 31, 2023

These all problem you can fix with single update button, i also facing issue in eric emanuel hoodie image design but i solve issues with the help of updates. Even you can also contact here for frimware team here https://firmwaresupport.com/

OrbiterAuthor
Associate III
July 31, 2023

?!  Where is that update button?