Skip to main content
Visitor II
October 8, 2024
Question

MCU SPC560B50L5 error: “Unable to enable OnCE 10-bit TAP controller Failed to connect. Could not perform custom sequence.”

  • October 8, 2024
  • 0 replies
  • 507 views

Hello.

I am using an MCU SPC560B50L5  in an LQFP144 package on the board, connected via JTAG. I'm trying using J-Link V11 SEGGER J-Link Registration V8.10 program.

When I try to connect, I get the error: “Unable to enable OnCE 10-bit TAP controller Failed to connect. Could not perform custom sequence.”

What to do for a ready connection?