Problem loading WAV files to AEK-MCU-C1MLIT1
Hello, I'm trying to develop an AVAS application, I have the AEK-MCU-C1MLIT1, the AEK-AUD-D903V1 and the AEK-CON-C1D9031 connection board. I've tested the Engine Sound Simulation and diagnostics with connection board and it woks, I get the sound out of the amplifier. However, when I try to change the audio files for ones of my own, I can't get any sound out of it. I proceed exactly as told in the instructions: I put the WAV files into the source folder (after checking they aren't bigger than 768kB), modify the sounddb.s file so it can access my WAV files, compile it, copy the .hex file from the build folder to the source folder and rename it, search for the 020000040100 string that identifies the beginning of the sound partition, delete everything behind that string, modify again the sounddb.s file so it doesn't compile the audio again, and then compile. It flashes without error into the MCU, but then it just doesn't sound. Could anyone help with that?
Thanks in advance