Skip to main content
acarn
Visitor II
October 10, 2019
Solved

SPC5-MCTK-LIB_RTM_1_1_0_web, lack of #include "pal_lld.h"?

  • October 10, 2019
  • 4 replies
  • 1188 views

Hello,

there's problem when trying to build the project (Regardless which of the Web Motor Control Demos I choose).0690X00000ApTKCQA3.png

The steps I made are:

1.) Import samples from application

2.) Choose one of the motor control applications

3.) Generate the SPC5 Application

4.) Build the SPC5 Application

The last step generates following error message:

./components/spc56xx_web_motor_control_component/lib/System_Drive_Params/src/Spc5xxx_MC_it.c:48:21: fatal error: pal_lld.h: No such file or directory

 #include "pal_lld.h"

Which is a bit strange, since I didn't make any changes to the configuration.

Can you please help?

    This topic has been closed for replies.
    Best answer by Erwan YVIN

    Hello ,

    1) MCTKLIB 1.1.0 is not compliant with SpcS5studio 5.8.1-Diadem

     There is Change Request to update the library .

    2) MCTKLIB 1.1.0 is compliant with SPC5Studio 5.8.1 (Old Version)

    http://mirrors.spc5studio.com/5.8.1/

    you can use it without updated RLA components.

    3) http://mctkcust.spc5studio.com is compliant with the last version but you need some credentials.

    to be asked in credentials@spc5studio.com

    Best Regards

    Erwan

    4 replies

    Erwan YVIN
    ST Employee
    October 17, 2019

    Hello ,

    i think that the web site is not updated .

    i have forwarded your request to the good person.

    Best Regards

    Erwan

    Czhu.844
    Visitor II
    November 6, 2019

    How about the problem? I also meet it ,help!

    Erwan YVIN
    ST Employee
    November 14, 2019

    hello ,

    after the next release of SPC5Studio , we will post a new release located in web update site

    Best regards

    Erwan

    a-daniel
    Visitor II
    January 22, 2020

    Hello,

    Was anything done about this ?

    I have the same issue with SPC5-MCTK-LIB 1.1.0 and SPC5Studio 5.8.1 .

    Erwan YVIN
    Erwan YVINBest answer
    ST Employee
    January 28, 2020

    Hello ,

    1) MCTKLIB 1.1.0 is not compliant with SpcS5studio 5.8.1-Diadem

     There is Change Request to update the library .

    2) MCTKLIB 1.1.0 is compliant with SPC5Studio 5.8.1 (Old Version)

    http://mirrors.spc5studio.com/5.8.1/

    you can use it without updated RLA components.

    3) http://mctkcust.spc5studio.com is compliant with the last version but you need some credentials.

    to be asked in credentials@spc5studio.com

    Best Regards

    Erwan