Skip to main content
TGecc
Visitor II
September 4, 2018
Question

spc5 studio can't detect my board

  • September 4, 2018
  • 1 reply
  • 739 views

Good morning

We connected the board spc570 by microUSB, our operating system (both windows 7 and windows 10) detected it as "SPC570S-DISP discovery board" but can't install any driver. We have already downloaded and installed SPC5 studio with "complete installation" but it seems that it can't be aware of the connected device: we can generate application code and compile a test application but we can't execute and debug it because execute and debug button remains always grayed. So we will ask if we have to buy something else or we have to download some specific driver or change some setting on the PC.

best reguard

    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Employee
    September 6, 2018

    Hello ,

    it is not SPC5Studio .. it is linked to PLS UDE

    PLS JTAG is integrated in your board

    Could you check with PLS UDE 4.10 ?

    https://www.pls-mc.com/login-a-384.html?User=SPC5UDESTKUser

    You have to install it

    • SPC5Studio is a Development Environment
    • PLSD UDE is used to debug and flash your binary

    Best regards

    Erwan