Solved
SPC5-UDESTK Serial Console ?
Posted on September 23, 2014 at 15:46
I am using UDE 4.2.05 with the SPC560B-DIS (which has UDE debug hardware built in)
I can load and run code via JTAG but ... How do I access the serial port connection to the target device ??? The target microcontroller UART is connected to the FTDI USB/serial/JTAG device but I do not see a COM port show up on the PC for the target USB/serial connection. Should this show up as a COM port or perhaps in a UDE window ??