SPC56EL Watchdog Timer Interrupt (IVOR12) triggering, but WDT not enabled?
I don't think I have a timer enabled. I don't see the WDT setting in the outline, but in the configuration.xml it is disabled. Most importantly clock_cfg.h is generated as '#define SPC5_DISABLE_WATCHDOG TRUE'.
However, almost randomly, I am getting an IVOR12 interrupt:
PC 0x00000380
CR 0x44000004
LR 0x00002D78
CTR 0x0
That said, the system runs for ten minutes, one minute, or five, then hangs up in IVOR12. The only driver I am using is the serial drivers, and may there is an issue there? It even triggers the ivor when degugging, which I thought the WDT was disabled for debugging as well.