SPC56xl FlexRay
Title: SPC56 FlexRay stays in startup (CSAA=1, STARTUPSTATE=5) with TJA1080ATS – static segment only, two ECUs, can’t reach Normal Active
MCU / IP: SPC56ELxx family (FlexRay controller inside SoC)
Transceiver: NXP TJA1080ATS (Channel A only)
Network topology: 2 ECUs directly on Channel A (no star coupler), proper bus termination added per TJA1080A datasheet
Bitrate: 2.5 Mbit/s (gBit = 50 ns µT; MT ≈ 2 µs; 40000 µT per cycle)
Firmware: Both ECUs built from the same project; only Frame ID / Key Slot differ per ECU.
What we’re trying to do
Bring up a small FlexRay cluster with two ECUs where both are configured as coldstart and sync capable (per FlexRay spec we plan for more nodes later). Each ECU transmits a static sync frame in its own key slot (Frame IDs differ). Static payload length is fixed and identical on all nodes.
Configuration (key parts)
Message buffers (RX filters):
-
MB[0] filters Frame ID = 1 (MBFIDR=1)
-
MB[1] filters Frame ID = 2 (MBFIDR=2)
-
MB[17] left as “all” / shadow config (MBFIDR=2047 etc.)
Key registers at runtime (examples):
-
PCR11.KEY_SLOT_USED_FOR_STARTUP=1, PCR11.KEY_SLOT_USED_FOR_SYNC=1
-
PCR18.KEY_SLOT_ID matches Frame ID per ECU (1 / 2 / 3 as tested)
-
PCR12.KEY_SLOT_HEADER_CRC prints as 1069 or 1586 depending on Frame ID (CRC code we compute is constant per header as expected)
-
PSR0.PROTSTATE=7, STARTUPSTATE=5, ERRMODE=0, SLOTMODE=2
-
PSR1.FRZ=0, CSAA=1, REMCSAT=1, CPN=0
-
PIFR1=0x1000, PIFR0=0x0001 (varies slightly between runs)
-
Debug outputs: CycleStart and SlotStart look correct; Syntax/Content error DBG pins show no pulses
Observations & measurements
-
On the scope, TXEN is controlled by the FlexRay peripheral and goes low before transmit; TJA1080ATS EN/BGE/STBN are held HIGH.
-
RXEN on TJA1080ATS is an indication output (not a control); we don’t drive it.
-
With proper termination fitted (per TJA1080A reference), the waveforms look clean.
-
Cycle timing: CycleStart and SlotStart spacing matches configuration (e.g., 100 µs between slot starts for gdStaticSlot=50).
-
Macrotick visibility on the debug pin: we observe ~1 µs pulses even though MT is configured as ~2 µs (gMacroPerCycle=1000 over 2 ms). The functional schedule timing (slots, cycle) still lines up with the config.
-
Frames transmitted by each ECU appear correct on the bus (header fields match, static payload length = 8 bytes).
-
Still, neither ECU reaches Normal Active. They remain with PROTSTATE=7 / STARTUPSTATE=5, CSAA=1, REMCSAT=1.
-
At some earlier point we had sum mismatch: static=800 sym=80 nit=113 -> sum=993 vs gMacroPerCycle=1000; this was corrected, and now the sums match (no current mismatch).
What we already tried
-
Verified all nodes share the same global timing (µT, MT, cycle, slot lengths, NIT, SW, APO).
-
Ensured identical static payload length across nodes (8 bytes = 4 words).
-
Confirmed unique key slots per ECU (PCR18) and both KEY_SLOT_USED_FOR_STARTUP/SYNC=1.
-
Checked Header CRC implementation (constant per header; matches between runs for fixed header).
-
Verified listen timeouts / noise parameters and increased pdAcceptedStartupRange to 1000 µT.
-
Confirmed bus termination per TJA1080ATS datasheet; verified clean signal edges; no obvious EMC issues.
-
Routed STBSCR DBG pins: CycleStart/SlotStart OK; Syntax/Content Error pins show no activity.
Questions for ST
-
With two nodes both marked as coldstart & sync (key-slot frames in static segment), are our PCR11 / PCR18 settings sufficient, or is there any additional requirement on SPC56 FlexRay IP to allow mutual startup?
-
Does STARTUPSTATE=5 with CSAA=1 indicate we’re transmitting CASs but not receiving sufficient valid sync frames from the other node? If yes, which RX filters / acceptance settings must be enabled for the controller to consider the peer’s sync frame toward startup (beyond our MB[0]/MB[1] filters)?
-
Are there mandatory values or minimums for gdSymbolWindow, gdNIT, or gOffsetCorrectionStart on this IP to pass the startup state machine, beyond FlexRay spec nominal ranges?
-
Is any clock/debug pin selection (STBSCR.SEL) or internal clocking option required so that the controller can measure/qualify the peer’s frame timing during startup?
-
Is there a recommended way to confirm that our Header CRC as written into PCR12 is actually being used/accepted by the controller during CAS generation and validation?
-
Any gotchas for TJA1080ATS with SPC56: required pull-ups/downs, split termination, common-mode choke, or BGE/EN/STBN timing relative to controller reset that could keep the controller in startup?
-
Are we missing the configuration of SFIDRFR.SYNFRID (currently 0) or any other register that affects recognizing the peer’s sync frames during startup?
-
Any checklist to explain why DBG Syntax/Content error outputs are quiet while we still fail startup—does that imply the controller simply doesn’t see a valid peer frame at the expected place?
Log snippets (representative)
Any guidance or a minimal working example for this IP (two-node static-only cluster) would be greatly appreciated!