Skip to main content
otcagon
Associate II
January 28, 2024
Question

SPC58-EC with Flash programming

  • January 28, 2024
  • 1 reply
  • 1390 views

Hello

I am try to apply flash code to my project but it shows strange behavior.

If I run run the code without break, program gose unhandled exception2.

If put some break points here, flash erase and flash program works well.

otcagon_0-1706408217909.png

otcagon_1-1706408251030.png

Left: Just before enter the flasherase routine.

Right: Programm in unhandled expetion2.

otcagon_2-1706408297081.png

I tried with some deliay routin just be break point, but the behavior is the same.

 

Are there any solution?

THanks

 

This topic has been closed for replies.

1 reply

otcagon
otcagonAuthor
Associate II
February 6, 2024

Hello, I check the other code run in ram. 

It works well and there are some comments for the execution of flash program must be run in ram.

I want to assign the function to ram but I failed because there is no C code delivered.

c55_freegcc.a, c55_gcc.a, c55_ghs.a are delivered so I cannot assign the funtion to ram using "__attribute__((section(".ram_code"))) ".

Are there any solution to run flash related code from ram. The other code runing at flash.

or if there are object code delivered with free assigned "__attribute__((section(".ram_code"))) " or the other, I ca

 

Thanks