SPC58EC-DISP Serial Communication Sample code HELP!!!
- August 24, 2021
- 7 replies
- 4483 views
A problem occurred during the serial communication test process with the SPC58EC-DISP board.
The test environment and problem symptoms are as follows.
test environment
1. Apply 12V Power to SPC58EC-DISP board
2. Debugging and Serial Communication Test through PLS USB Serial Port (COM6)
3. Using SPC5 STUDIO Sample Code ( SPC58ECxx_RLA_SERIAL Test Application for Discovery example code)
4. Checked the normal operation of LED of Sample Code (flash sample code using UDE STK )
5. Use Docklight to monitor serial communication from PC (Set as Baudrate:38400 Data bits:8 Stop bits:1 Parity:None)
6. Set COM6 PORT's Baudrate , data bits, stop bits from device manager
problem phenomenon
1. sample code is flashed on the board and then activated, the operation of sending Hello World through serial communication should be confirmed, but a strange value is sent and normal communication is not performed.
- It seems that serial data is being sent through UART communication with LIN Flex0 peripheral.
do I have to set something more set the jumper pin? If so, please let me know how to solve it and I will test it.
References is uploaded.
thank you