SPC58EG : Watchdog SWT example doesn't work
On SPC58EG, I try to use SWT
On SPC5 Studio6 , I use the example « SPC58xGxx_RLA SWT Test Application for Discovery »
In this example, it uses the SWT2, associated to core 2
When the emulator Lauterbach Trace32 is connected, the example works well
- The board does its 1st boot
- The watchdog SWT is refreshed few second
- The program stops refreshing watchdog
The board reboot (this is normal)
- The watchdog SWT is refreshed few second
- The program stops refreshing watchdog
- But the program an board continue run … (Why they are not rebooting)
When the emulator Lauterbach Trace32 is NOT connected, the example doesn’t work
- The board does its 1st boot
- The watchdog SWT is refreshed few second
- The program stops refreshing watchdog
- But the program an board continue to run. The board never reboots.
Why it doesn’t reboot, like 2sd reboot with trace32 ?