Question
SPC5STudio 3.4.0 is available !
Posted on January 26, 2015 at 16:57
SPC5STudio 3.4.0 is available !
Dear Users,
The 3.4.0 release is now available on the update site.Here are is the change logSPC5STUDIO CORE :- Patch mode: newly created project is already patched- Implementing invisible groups- Allow user to patch components/lib/ files: V2- Patch mode : patch.xml to be hidden / Default / Grey Decorators- Implement Hidden propertiesSPC5STUDIO Repository :- Create NIL RTOS SPC560Bxx Test Application for DiscoverySPC5STUDIO Pinmap :- Unable to Set more than 10 pin in PinMap WizardSPC5-HAL :- CAN Naming convention : Change the id number of Filter Settings- The message buffers Tx/Rx Configuration in CAN module are fixed- The incorrect registers bits definitions and driver data structures and types in hal_lld.h head file- eMIOS channels 1,3,5,6,2,4,11,13 are not usable for ICU- PWM/ICU functions on eMIOSNIL RTOS :- New feature for SPC560BxxWe wish you a happy usage.The SPC5Studio team. #latest-release