Skip to main content
GMG
Associate III
February 27, 2022
Solved

SPC5x pinout

  • February 27, 2022
  • 2 replies
  • 1476 views

Hi, where can I find microcontroller pinout?

I miss something? I can't find spc5 pinouts in datasheets, where are these resources?

Best regards​

    This topic has been closed for replies.
    Best answer by Giuseppe DI-GIORE

    Hello,

    for each SPC5 MCU pinout description is available in a specific technical note.

    See the MCU specific documentation page.

    For example, SPC58EC pinout is available in Technical Note TN1260 (link)

    Download the MCU specific I/O definition technical note, it is in pdf format,

    then the I/O pinout file is attached to the pdf as spreadsheet file.

    Regards.

    2 replies

    Giuseppe DI-GIORE
    ST Employee
    February 27, 2022

    Hello,

    for each SPC5 MCU pinout description is available in a specific technical note.

    See the MCU specific documentation page.

    For example, SPC58EC pinout is available in Technical Note TN1260 (link)

    Download the MCU specific I/O definition technical note, it is in pdf format,

    then the I/O pinout file is attached to the pdf as spreadsheet file.

    Regards.

    GMG
    GMGAuthor
    Associate III
    February 27, 2022

    thanks, opening the pdf from the browser it is not possible to see attachments and therefore I could not understand where they were.

    Giuseppe DI-GIORE
    ST Employee
    February 27, 2022

    Hello,

    please do not open the file in a browser, download it instead.

    Open with a pdf viewer, for example Acrobat Reader

    Open the left menu and click on the paperclip.

    0693W00000Kaim1QAB.pngRegards,