Skip to main content
Visitor II
January 13, 2025
Solved

SR6G7 Stellar BCS handshake and Custom Boot Manager

  • January 13, 2025
  • 1 reply
  • 1088 views

I would like to know, in the Stellar SR6G7, whether the BCS code will execute first or if we can configure a custom Boot Manager to execute first. Since I need to run secure boot with HSM, I want to configure the Boot Manager for PLL clock initialization and run the HSM first. Then, the BCS will execute the handshake with the HSM. Is this possible in the SR6G7, or will the BCS handle initialization and perform the handshake with the HSM during startup before any custom Boot manager?

Best answer by C.A-T.

Hi,

SR6 information is provided under NDA.
For any question, please contact local ST support, and do not post information/questions in this public forum.

Thank you.

1 reply

C.A-T.
C.A-T.Best answer
ST Employee
January 28, 2025

Hi,

SR6 information is provided under NDA.
For any question, please contact local ST support, and do not post information/questions in this public forum.

Thank you.