Question
System clock configuration
Posted on February 08, 2016 at 13:18
Good morning.
I have a problem setting the system clock of SPC560EL. I want to use the internal clock, but I cannot. Each time I execute the code, reading the main status register, I see that the SYSCLOCK switch to PPL. I cannot understand why this is the case.In the wizard, the external oscillator bypass is not checked. Is this the correct behaviour?Someone could be so kind to explain me how to configure the micro via wizard so that i don't use external oscillators? The board on which the micro is mounted doesn't have one.Thank you, Ivan #clock-generation-internal