The behavior of UART register of Chorus 4M
Hi,
I checked UART register of Chorus 4M my environment.
If I would like to set AUTOWU bit in LINCR1 register, is following sequence right?
linflexlp->LINCR1.R = 1; /* enter INIT mode */
linflexlp->LINCR1.R = 0x1001; /* set AUTOWU */
linflexlp->LINCR1.R = 0x1000; /* exit INIT mode */
When I wite '0' (0x00000000) to LINCR1 register to exit INIT mode like serial_lld.c in SPC5Studio (following), not only INIT bit but also other bits on LINCR1 register is clear. Is it right?
/* Leaves the configuration mode.*/
linflexlp->LINCR1.R = 0;
If it is right, I think it is very important behavior.
Best Regards,
Tsutsumi