Skip to main content
hans536
Associate III
October 26, 2022
Question

This is a purchase question aoubt spc58nh-disp flash module

  • October 26, 2022
  • 3 replies
  • 1357 views

I want to buy jtag module

when looking for it,

Looks like I'll have to buy the SPC5-UDESTK-EVAL.

(Is that right...? anyway...)

So I'm going to buy this product, but there are SPC56 and SPC57 in the description, but there is no SPC58.

Is it right to buy this product? Or do I have to buy another product?

This is the site you want to buy.

https://www.mouser.kr/c/?q=SPC5-UDESTK

Additional question.

Does SPC5-UDEDEBG upgrade the license period and write capacity of SPC5-UDESTK-EVAL?

    This topic has been closed for replies.

    3 replies

    Giuseppe DI-GIORE
    ST Employee
    October 26, 2022

    SPC5-UDESTK is the USB dongle for SPC5 debugging (suitable also for SPC58NH boards)

    Please have a look here: SPC5-UDEDSTK

    Best Regards.

    hans536
    hans536Author
    Associate III
    October 26, 2022

    I went to the site and there is no spc5-udestk, only spc5-udestk-eval.

    Can I buy this?

    Gaetano SANTORO
    ST Employee
    October 27, 2022

    SPC5-UDESTK-EVAL support SPC56, SPC57 and also SPC58

    Yes SPC5-UDEDEBG upgrade the license period and write capacity of SPC5-UDESTK-EVAL

    download software from https://www.pls-mc.com/service/downloads/download-spc5-udestk/

    then look at file:///C:/Program%20Files/pls/UDE%20Starterkit%202021/release.htm

    high end device like SPC58NH is supported but with following limitation:

    • SPC58NH84 (Cut1, only Core2)
    • SPC58NH90 (Cut1, only Core2)
    • SPC58NH92 (Cut1, Cut2, only Core2)

    see file:///C:/Program%20Files/pls/UDE%20Starterkit%202021/release.htm for all details

    Best regards