UDE STK 5.2 STOP WORKING AFTER FEW DAYS
Hi,
I'm currently working with a discovery board SPC58EC-DISP and I´m using a SPC5-UDESTK for debug, my issue is the next:
The first 2 - 3 days the UDE STK 5.2 works properly, I can connect to the board without problem, but after those days I am not able to connect with the board, it shows the next message

I delete and installed again the UDE STK 5.2 and I was able to connect to the board again but after few days Im facing the same issue, I have two laptops and in both Im facing the same issue, also the power supply and all the configuration is the same when it connects to the board and when it doesn´t connects, I read in some forums that it could be a power supply issue but definitely this is not the case because nothing changes when it works and when not..
also Im not the only one with this issue:
https://community.st.com/t5/microcontrollers/problems-with-ude-visual-platform/td-p/468544
Can you please help me?
Regards,
Elio Zepeda