Skip to main content
AChie
Associate
October 29, 2018
Solved

Unable to connect to SPC58EC-DISP board through UDE debugger.

  • October 29, 2018
  • 1 reply
  • 1450 views

I am trying to connect to the SPC58EC-DISP board through PLS UDE Starter kit to program and debug the Serial Test Application example provided with the SPC5 Studio IDE. After opening the debug.wsx in the example project file on PLS UDE, an error appears.(Seen in UDE error png and the connection failed report log)

I can see the devices connected through device manager as "PLS USB JTAG Adapter for SPC5xxxx A".

Please let me know why I can not connect to the boards.

    This topic has been closed for replies.
    Best answer by AChie

    Issue resolved. Got a new board and tested against it with the same configurations and it worked. Issue was with the original board I was working with.

    1 reply

    AChie
    AChieAuthorBest answer
    Associate
    October 30, 2018

    Issue resolved. Got a new board and tested against it with the same configurations and it worked. Issue was with the original board I was working with.