Skip to main content
davide23
Visitor II
January 14, 2016
Question

Using two FlexPWM modules with RPC56EL70L5 (SPC56EL70L5)

  • January 14, 2016
  • 1 reply
  • 669 views
Posted on January 14, 2016 at 10:48

Hi,

I am evaluating the use of RPC56EL70L5 to control two BLDC motors, using a FlexPWM module for each motor.

The datasheet of the SPC56EL70L5 states that the second FlexPWM is not connected to the pins of the package - the RPC56EL70L5 datasheet is not explicit about.

Is there a way to connect the second module (FlexPWM_1) to the output pins?

Any workaround?

Thanks, dave
    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Employee
    January 21, 2016
    Posted on January 21, 2016 at 18:18

    Hello Dave ,

    Sorry the RM is not clear.

    There is no FlexPWM1 on EL70.

    ''The pulse width modulator module (FlexPWM) contains four PWM channels, each of which

    is configured to control a single half-bridge power stage. One module is present in LQFP144

     

    package. Additionally, four fault input channels are provided per FlexPWM module.''

                                 Best regards

                                                     Erwan