WindRiver Diab with SPC5Studio - AN5171 - Compiling autogenerated rla c-files
Hi,
I followed the instruction in AN5171 to integrate windriver into the SPC5Studio DE.
When compiling an existing sample project for the SPC574K-DISCOVERY (SPC574Kxx_RLA PWM Test Application for Discovery) with the windriver diab compiler, it will throw a lot of errors.
1. Once the windriver plugin setup is correctly done, should all the autogenerated mcal code be directly compilable with diab, or is that not supported?
2. What must be done to configure SPC5Studio to generate diab compatible c-code?
Best regards
Norbert