Skip to main content
Umahe.1
Associate II
May 20, 2022
Question

Analyze is failing with keras(.h5) model and throwing INTERNAL ERROR: The layer has never been called and thus has no defined input shape.

  • May 20, 2022
  • 0 replies
  • 758 views

I have a model file(.h5) and Analyze is failing with keras(.h5) model at STMCubeMX and throwing INTERNAL ERROR: The layer has never been called and thus has no defined input shape.

Need help in understanding the issue and resolution for the same.

My model is attached here for reference

Thanks in Advance

    This topic has been closed for replies.