Skip to main content
Associate III
July 4, 2025
Question

Automode, logger seems to log but not enough data in the SD card

  • July 4, 2025
  • 3 replies
  • 403 views

Hi,

I'm using the STEVAL-STWINKT1B and the automode to log data, with the FPSNSDATALOG2 firmware. I'm reaching out because, although the logger seems to run for multiple hours, I only get a few minutes (or at best a couple of hours) of data saved on the SD card.

Here’s what I did:

  • I charged the dev kit's battery for about 7 hours. Before logging, the ST BLE Sensor app showed the battery level at 95%.

  • I formatted the SD card to FAT32 with a 32K allocation size.

  • I copied the following device_config.json to the root of the SD card:

    • nof_acquisition = 0

    • logging_period_s = 900 (15 minutes per file)

  • I started the logger by pressing PWR and RESET. The green LED blinked at 4Hz, indicating logging had started.

I monitored the logger as much as possible. After 8 hours, the green LED was still blinking, and the ST BLE Sensor app showed:

Alarm: Logging ongoing
Battery: 55%
(see screenshot below)

anthonyADV_1-1751616933611.png

However, when I checked the SD card, I only found about 2.5 hours of data, specifically, 10 folders of 15 minutes each. But I expected at least 8 hours of logging.

anthonyADV_2-1751617188679.png

So my question is: Why do I only get a few hours of logged data, even though the logger appears to be active (green LED blinking) for much longer?

Additional notes:

  • I repeated this test several times, and the result is always the same: much less data on the SD card than expected.

  • Here's the battery level over time during the abovementionned test:

    • 0h: 95%

    • 5h: 65%

    • 5h15: 61%

    • 6h: 60%

    • 6h30: 58%

    • 7h46: 55%

  • I’m still using the SanDisk Extreme 256GB SD card (SDSQXAV-256G-GN6MA). I’m aware this is not one of the cards officially tested with the STEVAL-STWINKT1B, alas, I haven’t been able to get a different one yet.

Thanks in advance for your help !

Best regards,
Anthony

3 replies

Associate III
July 22, 2025

Hey, just a quick follow-up, I still haven’t found a solution. Thanks in advance

SimonePradolini
Technical Moderator
July 23, 2025

Hello @anthonyADV 

Sorry for the late reply. I'm launching a 24-hours test session and come back to you soon.

 

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SimonePradolini
Technical Moderator
July 30, 2025

Hello @anthonyADV 

I tested different SD cards and power supply setups. I can't find any issue while using an external power supply or a power bank via USB. Instead, I got your same undesired behavior with a couple of SD cards with the board battery-powered.

While acquiring data on the SD card, the firmware checks for the battery status: if it detects something not working properly (battery discharge, low battery percentage, ...), it saves data and closes the acquisition. This is a safety procedure that we implemented to avoid broken data acquisition due to a power supply failing.

My suspect is that there’s an issue in the battery status check: I'm debugging there, wishing providing you with a solution soon.

 

Thanks for your feedback on our products. I really appreciate your job

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate III
August 11, 2025

Hi @SimonePradolini,

Got it, I’ll wait to hear back from you :) I’ll keep going with my recordings using a power supply setup.
Can I ask which power bank and/or external power supply you used for your tests? Mine tends to shut down unexpectedly, so I’ll probably get the same as yours to make sure I don’t run into issues.

Thanks a lot for your replies!

Best,
Anthony

SimonePradolini
Technical Moderator
August 12, 2025

Hello @anthonyADV 

I'm using a generic one, a USB power supply from a smartphone. Are you still in trouble? Do you have the same undesired result also by reducing sensors ODRs or by disabling some of them? For example: what if disabling IMP23ABSU and IIS3DWB at all?

 

Best regards

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.