Skip to main content
ADe V.1
Visitor II
April 30, 2023
Question

Comm_Interface column in .txt data log generated by Unico does not allow to upload the data for MLC

  • April 30, 2023
  • 0 replies
  • 955 views

Good morning,

I'm having some issues with the MLC configuration of a LSM6DSV16BX sensor through Unico GUI.

I've followed the tutorials provided by ST online and I've looked through the related GitHub repository, but, when I save a datalog through Unico GUI, the .txt file seems to have an additional first column of data called "Comm_Interface", which takes the value "UI" in each row.

When I try to upload the data to the MLC section of unico, all the values are seen as 0: by manually eliminating the first column (which is not present in any of the examples that were provided), the values are interpreted correctly.

Is there a reason why such column is added to the .txt file? I couldn't find any examples with this same issue and I'd like to know if the file can be saved correctly, thus removing the need to modify it before using it (especially since I'm using the same platform to log and analyze the data).

Thanks in advance for the help!

This topic has been closed for replies.