configuring STM32N647X0H3Q using STM32CUBE AI STUDIO

As shown in the figure, I have equipped the MCU with an external FLASH connected via XSPI2. However, it seems that AI Studio is not aware that there is an external FLASH. How should I configure it to solve this problem?


As shown in the two pictures above, after I connected the development board via ST-link, I wanted to run it on the target, but it prompted "failed to start running". Why is this happening?